Axis Limits Parameters

Servo Axis - Axis Limits

Figure 5-26: Servo Axis - Axis Limits

The Servo Axis - Axis Limits parameters are:

Parameter Description
In Position Tolerance The maximum distance between the axis's actual position and its commanded endpoint for the axis to be considered “in position”. The In-Position Tolerance is specified in User Units.

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen